This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Current sense resistor value

Part Number: BQ34Z100-G1

Hi team, 

I am working on a 131V battery pack with a max current output capability of 80A. I used a 2mohm sense resistor and for the load drawing 5A (tried to calibrate current keeping 5A max current output as of now, and hence gave no scaling factor), the current reported by the gauge is around 60A. Kindly tell me if the resistor value is too small and that we need an opamp or am I missing any calibration step. 

I calibrated CCGAIN, CCOFFSET, BOARD OFFSET followed by current. 

Thanks,

Shreya