Hi Team,
Kindly help here in verifying our circuit.
We are using the IC LM5143-Q1 in our design.
Specifications of our circuit is the following
Vin = 6V to 30V
Vout1 = 5V, 9A
Vout2 = 3.3V, 9A
The MOSFET that are connecting in the pins HO1, HO2, LO1 and LO2 is BSZ100N06LS3GATMA1. Could we know whether this MOSFET suits our design and also confirm us the attached circuit is fine or not
Thanks in advance.