We are using Type-C DFP Controller for Charging, and I need to know the functionality behavior of CC pins. In our scenario without connecting the Charger cable both CC1 and CC2 are getting high (whether this has internal pull up to IN2?), and after connecting a device for charging both the pins are getting dropped to 0.92V and 1.2V(Why this is happening?), So I need a clarity on how it behaves because there is no proper information about CC pins in datasheet.