Other Parts Discussed in Thread: BQSTUDIO, GPCCHEM, BQ40Z50, BQ78Z100, EV2400
Hello all,
I have recently done a design using a BQ28Z610 fuel gauge to protect and monitor two series cells of 6000mAh Li-Po batteries. I have succesfully completed a learning cycle of the battery module. I assume the learning cycle was successful as I followed the guide, and the Update Status is currently set to 0x0E. From what i understand from this chip, the update status register should not be manually edited in the .GG file after the trained file has been exported, so I have kept this value at 0x0E when i import it to my other BQ28Z610 battery gauges.
When the module is used in our product, it seems like from time to time the battery SOC jumps to 100%, and sometimes it stays there for a long time (even when draining the battery). When connecting to the device, using bqStudio, i can see from the pack and cell voltages that the battery is clearly not 100%. If i send a soft RESET command through bqStudio, the device will reset and the next read will show a lower SOC (some number that seems more realistic).
Does anyone have any experience with this issue? Have i missed something/done something wrong during the training cycle of my initial module? Is there any values that should be manually set in the .gg file after the export of the file?
I will attach an image of the circuit around the gauge:

Any help would be greatly appreciated!
Best regards,
Sondre