Hi team,
Based on some special working conditions(they said the Vsys would be 19V in some condition and the BAT pin could stand 20V, they worry about the margin) , the customer has made the following design:
A switch(mos) is added between the BAT pin and the battery. When not charging, disconnect the switch between BAT and the battery, and the battery is directly connected to SYS; when charging, close the switch, which means that SYS and BAT are connected in parallel to charge the battery.(btw, can customer use the SDRV pin to control the mos as they want to add)
Please help the customer to evaluate whether there is a problem with this use, and whether it will affect the charging control of the chip.
Yours
Nan