Other Parts Discussed in Thread: SN65LVDS2, SN65LVDS1
We are using a cascaded configuration of TPS7A4501 to supply 2x SN65LVDS1 and 2x SN65LVDS2 so around 30mA max.
As we are powering the circuit in sequence and we can't soft start this part, we have stumbled upon a problem because the second LDO is inducing a high spike of current to the recommended 10uF low ESR output capacitor which can induce a glitch in the LDO upstream and trigger our voltage monitoring device into a reset due to the voltage brown-out.
The solution found was to remove this output capacitor and the circuit seems to still be stable at both 60°C and -40°C.
Our question is, is it not recommended to use the circuit in this configuration without this output capacitor or should we replace it with another capacitor given the circuit described here. The C9 and C10 are low ESR ceramic capacitors.
Here are some measurements and simplified schematics attached to illustrate. We can see the ringing is way less present without it.
Thank you