Hi!
We have a project were we've used LP87524PRNFRQ1 configured in the following way:
Buck0: 0V85
Buck1: 0V9
Buck2: 2V1
Buck3: 1V8
Currently we no longer have the need for 0V9 rail on Buck1 output of the LP87524PRNFRQ1 and so we would like to remove all components related to that output. We would like to keep the LP87524PRNFRQ1 because of other reasons.
Is it OK to leave the pins SW_B1, FB_B1, VINB1, EN1 floating or should we connect them in some other way?
Is there something else we need to take care in HW design to support 3/4 outputs?
Is there any documentation reference to this state?
Best regards,