Hi Sir,
I am using tps43060 drive the mosfet BSC098N10NS5 and find that the low side gate is very hot and the gate rise time is very long(I think it should shorter).
Desgin input: 19V input, 54V1A output
MOSFET Qg total: 25nC max
Frequency: 450kHz
The question is the gate rise time is about 300ns and it is longer than I expected which should be about 100ns?
I think there is some problem with the layout, but I am not sure what cause the rise time unexpected?
Best regards,
Xiangnan