This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5036: max vled?

Part Number: LP5036


Hi Team,

what is the maximum vled voltage for LP5036?

If several diodes in series are being used can I assume that vled can not be higher than the sum of all forward voltages in series + Vcc?

BR,
Stefan

  • Hi Stefan,

    The maximum vled voltage is 5.5V:

    So, we don't recommend using several diodes in series.

    If they want to connect several diodes in series, you can looking for the backlight driver with higher Vout.

    Thanks!
    ives Li