Hi team,
In the datasheet, Ilim_SW is specified as below.
Does min, typ, max value changes with the RLIM value? Is ILIM_SW only determined by the ISEL high lor ow?
Also, for ILIM, can it alway be set to 0.1A~3.0A regardless of ILIM_SW?
I know that in the datasheet, it says:
"The current limit can be programmed from 0.1 A to 3.0 A. It is recommended to set ISEL pin logic low when setting input average current limit below 750 mA.".
But as an irregular case, can ILIM be set higher than 2.5A when ILIM_SW is 2.5A with ISEL low?
Regards,
Ohashi