This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ways to reduce the current limit threshold of TPS 54231

Other Parts Discussed in Thread: TPS54231

Need help to reduce the Max. current Limit Threshold of the device as per below specs .

Vin: 12.5-20 V

Vout: 11.3 V

Iout: 2.5 Amps.

Max Peak current limit threshold: 4.5 Amps.

Iout ripple: 0.1 Amps.

Vout ripple: 100mv

If anyone knows the wayout to reduce the current limit threshold of 5.4 Amps of 54231 than pls. help me out.