Hi,
Good Day.
The customer is looking for Power Path Controller/Switcher that can switch between three sources.
He saw a few eFuses, those in the Oring application would be an alternative but mainly it's around 300W switching between three input sources.
Thus external MOSFET option is a must, something close to LTC1479.
I suggest the TPS2113A but LTC1479 isn't close to the solution I have provided.
It does not match three input capabilities with the external MOSFET option for higher current switching.
5.5V, 1.25A switcher is not equivalent to +300W switching.
He is looking to switch currents of excess of 25A with Voltages of up to 18VDC.
Maybe there is a solution using a combination eFuses with Power.
Please advise. Thank you very much.
Best Regards,
Ray Vincent