Part Number: BQ24075
Other Parts Discussed in Thread: BQ25180
Hello TI gurus,
I'm desiging a project with this IC in for power path management and charge management of a 1200mAh battery. It's paired with an STM32F405 microcontroller.
Basic design is that a keypad button is connected via a diode to the SYSOFF line, so that when you press the power button on the keypad, the SYSOFF like is pulled low, and powers everything on.
The micro boots, and then switches on Q2 (on the above schematic) and also pulls SYSOFF low. When the user releases the keypad, the system then remains on.
At some point, when the user wishes to power down, another push of the power button is seen by the micro through a second diode. It does housekeeping, and when it's ready it can let go of SYSOFF and power off.
There is a second MOSFET on the SYSOFF line from the USB, so that when the USB is connected, the system immediately powers on, and stays on as long as the USB is connected. This is to allow the micro to control and monitor the charge process.
The output from the BQ24075 is connected to an ULDO 3.3V regulator to provide a reasonably stable supply to the rest of the system.
For the most part, everything seems to function as intended, howver, occasionally the BQ24075 seems to randomly switch on, and won't switch off.
I originally thought it might be a bit of charge leakage through the micro, and causing it's output transistor to flick on enough that it's pulling SYSOFF low enough that it's causing a poweron, and then latching it on (I originally had the micro directly connected to SYSOFF with an open drain output), but putting a MOSFET between the micro and the SYSOFF line (with a strong pulldown to bleed away any excess charge) doesn't seem to have fixed it. It's a bit random (I haven't yet noticed any kind of pattern to times etc) and can be any time between a few minutes or hours, if it happens.
When it's not doing silly things, it's working beautifully, charging the battery, powering on / off as expected.
Any suggestions?