Part Number: BQ76952
Hi Team,
My customer wants to ensure that the minimum cell voltage is above a certain level during cell balancing, for example, if minimum cell voltage drops below 3.6V, BQ76952 would stop balancing.
According to BQ76952 TRM, BQ76952 would ceases balancing if all cell voltages are within Stop Delta of the minimum cell voltage.
It seems that it would not take the minimum cell voltage as a condition of stopping balancing. To stop balancing, BQ76962 would only take the voltage delta as the condition.
The questions are-
How to prevent the minimum cell voltage dropping too low during balancing?
Is it possible to set two different minimum cell voltage values for entering/stopping balancing? (e.g., 3.8V for entering, 3.6V for stopping)
Regards,
Charles