This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62084: output ripple at low current

Part Number: TLV62084

Hi Team, 

Could you please kindly help test Vout ripple at below conditions? Thanks. 

VIn = 3.6V,  3.8V, 4.2V 

Vout= 2.8V

Iout=100mA

L= 1uH,  Cout= 10uf + 22uf, 6.3V, 0402 package. effective capacitance is 40%* nominal cap value. 

I have applied for EVM but it takes time, please kindly help check on this. Thanks. 

BRs

Given