Other Parts Discussed in Thread: TPS2812
Hi,
Can UCC2808A-2D is supplied from LDO in TPS2812D?
- Input Voltage : typ 24V (10.8V ~ 30V)
- Output Voltage : 48V
- Pout : up to 150W
Webench recommended UCC2808A-2D and TPS2812D.
However, input voltage exceeds UCC2808A-2D input range and it needs another supply.
TPS2812D has internal LDO and output is 11.4V.
Can it be used for UCC2808A-2D VDD?
Thanks.