Part Number: UCD3138064
Other Parts Discussed in Thread: UCD3138, , UCD3138PSFBEVM-027
Hi TI Experts,
-
We are planning to construct an interleaved PSFB (two phase, 180 degrees). Each phase will have its own 400Vdc input, and these will be combined to produce a 12V output at a maximum of 375A.
-
I have a few questions about this:
-
Is it possible to use two UCD3138064s (64-pin + 40-pin) for the interleaved PSFB? Can they be connected with SYNC? Is there an example that shows how two UCD3138 devices can synchronize their phases (and delay)?
-
Can one UCD3138064 handle the feedback control, with the other following its duty cycle? This way, I wouldn't need to worry about current balancing.
-
Let me know if you need further clarification on any points. Thanks a lot.