Hi,
I want to design a custom SMPS with the required specifications:
Input voltage min: 22V; Input voltage max: 26V (Nominal input: 24V)
Output voltage: Isolated 150-0-150V (With center tap transformer)
Output power maximum: 25W
Output voltage should be adjustable with Master controller/ Digital potentiometer (Positive and negative voltage will be in sync. So, only voltage feedback of positive voltage is enough).
Output current threshold should be adjustable with Master controller/ Digital potentiometer (0-200mA with precession of 5mA).
If you have any design, please reply back.
Thanks...