This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25750: How to detect Sink Standby

Part Number: TPS25750

According to the PD standard, the Sink shall implement a mode called Sink Standby, with requirements that power consumption is below 2.5W.
I'm struggling to find any register values that do represent this status in the TPS25750. Could you please advice how I can get this status from the TPS25750?

I do find something in register PD status in the Host Interface Technical Reference Manual, but this has the wording "Received a GotoMin message unexpectedly.", so it seems like this is only activated during an error condition?

Best Regards

Vidar