This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A74: Schematic review and question on Css

Part Number: TPS7A74


Hi Team,

Could you pls help review the schematic, and I have 2 questions here:

1, What's the risk of having a capacitance greater than 15nF on the SS pin? Could you please clarify.


2,I think a capacitor to ground helps reduce noise. But what is the role of the capacitor from Vout to FB, and is it recommended to add it?

F1,5V to 3.3V / 0.14A, TA=105℃

F2,3.3V to 0.8V / 0.14A, TA=105℃

F3,3.3V to 1.8V / 0.546A, TA=105℃

Regards,
Hailiang