Other Parts Discussed in Thread: UCD3138
Hello,
I'm trying to use the UCD3138HSFB-029 in CC mode but it doesn't work.
Here is the setup:
UCD3138HSFB-029 powered with 45Vdc, 4A limitation. Load: variable resistive load (11 Ohms max)
in GUI Fusion: CP limited to 15W, CC limited to 1.5A and CPCC enable.
When starting up the UCD, I have 12Vdc output, in CV mode.
When the load current reaches such a level to have full power as specified in GUI Fusion (15W), the output voltage to be regulated reduced, the higher the load current, the lower the output voltage regulation point, in this way, the constant power operation is achieved. --> CP OK.
From this point, if I increase the current to go to CC (reduce the resistive load), the power stage stay ON for 2 secondes, then stop for 1 seconde then retry for 2 secondes ... And so on.
Is this comportment the hiccup mode ?
If yes, it seems to be in contradiction with the EVM user guide wich says "In hiccup state, the power stage stays on for 1s, and then goes to idle state and try to turn
on again."
I looked for the primary current if the cycle-by-cycle current limit was triggered but the inrush curent is always lower than the limit (16A)
I understand thanks to several answers in TI.E2E forum that CPCC module is not a good choice to work in CP or CC mode, and the firmware function developped in EVM firmware standard_interrupt.c is better. Do you have any application note with this function ?
Can you please help me to maintain a constant current ?