When I began looking for a current-limited load switch I found TPS22950-Q1. It is only available in SOT23-6.
Recently, the TPS22950 datasheet was updated to add the SOT23-6 package for the non-automotive part.
I am not seeing any significant functional difference. For example, Iq,VIN is 44uA typical vs 40uA and the OQD resistance changes a bit with supply voltage above 1.8V and the switching characteristics are a bit slower for the automotive part, but those differences are small and aren't significant to me. (If they are even real.) Is there a notable functional difference between the 'regular' TPS22950 and -Q1 version? Ultimately, I'm wondering if I can also use the non-automotive part in my non-automotive application where the regular TPS22950 is otherwise suitable.