We are using the TPS51200DRC DDR4 Termination Regulator in one of our designs. The regulator seems to work fine at room temperature, and we have 0.6 V output from V) and REFOUT, but once we get hotter (> +30 degrees C ambient), Vo will begin to pulse. The pulse will come up from 0.6V to about 1.0V repeating about every 1.2 seconds. We put a thermocouple on the LDO case, and it was pretty hot at about 107 degrees C. I would not expect that it would be going into a thermal shutdown, but I guess it is a possibility since the junction temp would be quite a bit higher than the case temp. What type of behavior would you expect with an overtemp condition? Would it pulse high like we are seeing? I would think that the output voltages would drop out to 0 V if an overtemp shutdown occurs. Any help or suggestions would be greatly appreciated.