This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HD3SS3220: CURRENT MODE pin setting

Part Number: HD3SS3220

Hi,

In default application, current mode is pull up to VDD, 5V power rail.

If customer wants to use 3.3V pull up, whether it is okay to adjust pull up resistance in same divided voltage compared to VDD?

Thanks and Best regards,

Tiger

VPU 5 3.3 V
Rtop 500 127 Kohm
Internal pull down 250 Kohm
Current_Mode
pin voltage
1.666667 1.6764 V