Hello,
I made a prototype board which uses the BQ27742-G1 and was unhappy to find that I must attach a charger or short Pack+ and Cell- according to Section 2.1 of the eval board's user guide. https://www.ti.com/lit/pdf/sluuax8 else I can't power my circuit. Is this mentioned anywhere in the actual datasheet? I would have thought if I was within the required voltage ranges, I could power the circuit when attaching a battery.
Anyways, I'm curious what is the design intent for this for startup/shutdown. I'm guessing the intent was to have a connected LiPo at all times and never disconnect, but have low-voltage cutoffs like the one included in the BQ27742-G1. Aren't there any worries about the LiPo continuing to drain through leakage currents? I see this all the time with old smartphones, that I can't even power on, even with a charger attached, after they've sat in the closet for a few months.
I'm working with a LiPo powered device that can see anywhere from a few minutes to several months of down time. So we're trying to implement a rocker switch (or similar) to completely cut off the cell from the rest of the circuit to prevent as much drain as possible, while keeping it safe from undervoltage dangers. Since the BQ27742-G1 cuts everything off, then even with a full battery, I switch on the rocker switch, my host controller will never be powered, so I can't do anything from the firmware side of things. So I guess I can use one of those 3-position rocker switches that push-release to short these two terminals and the other two positions would be the normal connect/disconnect. Is that a viable option for this or would this cause trouble somehow I'm not foreseeing? If this is seen as an issue, could you please provide a viable alternative?
Best regards,
Christopher