Hi,
I followed most of the sample circuit given in datasheet with unused inputs pulled low and outputs left floating.
I want to convert from 15V to 5.7V. As Vin reaches 15V, the power on sequence does not complete, it seems to be stuck in the Init stage and does not proceed to the ramp stage. Vfb stays close to 0 and Vreg only measures 1.75V, not the typical 4.5V.
Is there a reason Vreg would not be able to reach 4.5V if the only thing connected to that pin is Vreag_q and a 4.7uF cap? Thanks.