Hi,
My customer is designing the following:
- Device : TPS62147 @ 1.25MHz SW-Freq
- Inductor : 2.2uH
- Input Voltage : 5V
- Output Voltage / Current : 1.0V @ 0.9A
- Output capacitance : C1:44uF near inductor and C2:491uF(total) for next ICs.
On the above case of short distance between C1 and C2, total is 535uF. On this case, could you please let us know any issues?
If the above case has any issues, do they resolve this issue to add ferrite bead between C1 and C2? Please advise us.
Thanks and best regards,
M.HATTORI.