Hey Team!
Working with this PSPICE model and running some output ripple tests. I noticed that the frequency of waves of the switch node is off. Instead of being ~526kHz, it's ~5/6MHz:




This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Team!
Working with this PSPICE model and running some output ripple tests. I noticed that the frequency of waves of the switch node is off. Instead of being ~526kHz, it's ~5/6MHz:




It's the built-in model for the device:
I just edited the load, R1, and the inductance to match some specifications.
Hi Randy!
I just guess the waveform you measured is during start up. Could you waiting more time and measured the steady state?
Shuai