This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2596: Build a complete non-isolated AC/DC converter using the LM2596

Part Number: LM2596


Hello,

I am looking to build a cheap and simple non-isolated, completely transform-less, AC to DC converter using the LM2596. To do this, I am thinking to add a PFC converter as a front end to the LM2596.

Can any one suggest a suitable PFC converter to complete this design?

The power supply specs are:

Input: 180 - 250V AC

Output: 12-24V DC, 2A nominal (3A surge)

Thanks in advance

Mohamed