Hi Team,
My customer is using the device in the following environment as a test.
Vin:11.4V、12.0V、12.6V
Vout:5.0V
Iout:0A~Over current condition (with electronic load)
Temp:80℃
They reported current limit was observed at around 2.33A instead of 3.3A mentioned in the datasheet, with the inductor current as below.
The device's current limit back to 3.3A under room temperature.
Does the ambient temperature affect the current limit value? I only see the datasheet test condition was junction temperature -25C to 125C.
Regards