This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z80A-V110: bq20z95 .gg file data flash registers different in 2010 vs. bq29z95 .gg file data flash registers in 2023

Part Number: BQ20Z80A-V110
Other Parts Discussed in Thread: BQEVSW

Comparison of a .gg file for a bq20z95 in 2023 shows 9 additional data flash resisters beyond the .gg file for a bq20z95 in 2010:

Class Subclass ID Subclass Offset Name Data Type Min Value Max Value Default Value Units Name Value
                      [IT Cfg(Gas Gauging)]  
Gas Gauging 80 IT Cfg 0 Load Select U1 0 255 3   Load Select  3
Gas Gauging 80 IT Cfg 1 Load Mode U1 0 255 0   Load Mode  0
Gas Gauging 80 IT Cfg 45 Term Voltage I2 -32768 32767 12000 mV Term Voltage  12000
                    Res Current Rate  10
                    Q Invalid MaxT  40
                    Q Invalid MinT  10
                    Min % Passed Chg for Qm  37
                    Qmax Filter  96
Gas Gauging 80 IT Cfg 60 User Rate-mA I2 2000 9000 0 mA User Rate-mA 

0

Class Subclass ID Subclass Offset Name Data Type Min Value Max Value Default Value Units Name Value
                      [State(Gas Gauging)]  
Gas Gauging 82 State 0 Qmax Cell 0 I2 0 32767 4400 mAh Qmax Cell 0  13090
Gas Gauging 82 State 2 Qmax Cell 1 I2 0 32767 4400 mAh Qmax Cell 1  13090
Gas Gauging 82 State 4 Qmax Cell 2 I2 0 32767 4400 mAh Qmax Cell 2  13090
Gas Gauging 82 State 6 Qmax Cell 3 I2 0 32767 4400 mAh Qmax Cell 3  13093
Gas Gauging 82 State 8 Qmax Pack I2 0 32767 4400 mAh Qmax Pack  13090
Gas Gauging 82 State 12 Update Status H1 0x00 0x03 0x00   Update Status  2
                    Cell 0 Chg dod at EoC  0
                    Cell 1 Chg dod at EoC  0
                    Cell 2 Chg dod at EoC  0
                    Cell 3 Chg dod at EoC  0
Gas Gauging 82 State 21 Avg I Last Run I2 -32768 32767 -2000 mA Avg I Last Run  0

The new registers are not listed in the latest Tech Ref manual sluu264B

What is the functionality of the new registers and when were they added?