Part Number: TLV61048
Hi guys,
The following is the relevant section of my schematic:

When the TLV61048 gets 5V, it releases smoke.
The issue can be reproduced when the circuit only contains the TLV61048 and the NRS5020T3R3NMGJ inductor. Only VIN, EN, GND, and SW are connected. FREQ and FB are unconnected. See the following breadboard:

Thanks for your help in advance!
- Laci