This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM63606: TPSM63606 TPS25981 Power Sequence

Part Number: TPSM63606
Other Parts Discussed in Thread: TPS25981

Hello, 

I am planning on using the TPSM63606 DC/DC and would like to power on after TPS25981 eFUSE is enabled and the PG line is asserted. My voltage in is 12V and the output voltage from the DC/DC will be 5V. 

My initial plan is to enable the eFUSE based on the the input voltage between 10-14Vdc, one the PGOOD line is enabled I would like to toggle the enable pin on the DC/DC to start it up. However the eFUSE PGOOD is only rated to 5V so cannot tie it to the input voltage. My question is can the DC/DC VCC be used as a voltage source to pull up the PGOOD line. I am unsure if the LDO is fed from the input voltage or output voltage of the DC/DC.

Below is a simple picture. Biggest thing is the VCC needs to be at 5V so the Enable line could be pulled high.