This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5070: POE transformers for LM5070 controller

Part Number: LM5070
Other Parts Discussed in Thread: TPS23753A

Hi, 

I have a question regarding LM5070 for this requirements

POE requirements  V out: 12V, 1A. Where to look for POE transformers for this controller and what characteristics to check? Is this solution suitable for the new products or there are better alternatives?

Julia

  • Hi Julia,

    Coilcraft's C1586-AL is a transformer that was specifically developed for use with the LM5070, and meets your 12 V, 1 A output requirements.
    For other transformer options, I would check for a flyback transformer suited for 13 W applications,  with the 12V, 1A Vout. You can refer to the datasheet for the C1586-AL to compare.

    The LM5070 itself is one of our older products, a newer product that has similar function would be the TPS23753A, if you were interested in looking at newer products.

    Hope this helps.

    Best,
    Sarah