Hello,
About the BQ7721605 secondary protection. It has a timer that when one of the cells is above 4.225V then the timer starts and if one of the cells remains above 4.125V (it has 100mV hysteresis) for 1 second than the IC trips. To reset the timer before he reaches to 1 second, i need to go under 4.125V in all of the cells. When all of the cells goes below 4.125V, after how much time the timer is reset? 50ms?
Thank you