Hi everyone,
I'm having a problem with a new bq78pl116EVM that was just purchased. The device worked correctly for the past few days and all setup procedures were followed properly. tmap files were created to match the number of resistors to be used as a cell simulator. Just today, I checked to see how the system dealt with an open circuit by removing one of the resistors in series. Once it was removed, the fuse blew and the system seemed to go into a shutdown state. After turning off the power and trying to restart the EVM and software, the software tries to initialize and reports that it cannot read the parameters from the board. It cannot recognize any of the 'cells' attached to the board as well. It can still poll data from the board such as status flags but does not send any cell data. For reference, the VLAN failure flag is red and the fuse and precharge FET have green status indicators.
After going through multiple troubleshooting steps, I'm at a loss as to what has caused the board to fail to operate. Any insight into what may have failed or what should be reset would be very helpful.
Thank you,
-Andrew