Other Parts Discussed in Thread: TPS63000
Hello,
I got this demo board and configured it to run with the INA180A1 in a constant current mode.
I am happy with the performane with the circuit, when I open the LED load the TPS63000 will be damaged!
see. fig 5.1
The FB pin is used for the current control, but can I also use this pin to set the output voltage
so the device don't get damaged. If so how?
Thanks,