I am currently designing a PCB with an LM5146 and am using the LM5146Q1 development board as a reference. The schematic of the PCB shows TI routing the LO output of the IC under the VCC-GND cap. However, the HO output of the IC is routed with a via because TI uses a resistor in series with the bootstrap capacitor. If I only use a bootstrap capacitor with pads of sufficient separation, am I able to route the HO output under that capacitor without issue? Why or why not? Here is a picture for reference.