Hello to All,
for a new project (Vin=48V (-15% and +10%), Vout=34V, Imax=15A, EN55022, class B), I'm trying to use the active EMI feature, but I don't understand very well (or I don't want accept the real reality), if I need to apply to VCCX the external 5V or can I connect this pin to another pin (Vcc: is it output?). But reading the data sheet, the Vccx-max is 6,5V... Considering the Vin(max) is near 60V, I need a regolator from 60V to 5V...
Please, someone, clarify me...
Federico