This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92520-Q1: output current accuracy and calculation

Part Number: TPS92520-Q1


Hello expert,
   In my design the power coil is 47uH,current sample resistor is 0.1R.Input 30~60V,output 3~50V 0.1~1.5A.Tj -40~150C

  Could you pls share the output current accuracy and calculation for this device? 

  

  • Zhiyuan,

    We clearly state that at full scale voltage which is controlled by registers, that a +/4% accuracy is ensured.  

    We actually test each part such that at full scale (1023 setpoint) it is within our tolerance of +/4%.  Here is the specifications that references that test.

    Keep in mind that this doesn't include the current sense resistor tolerance.  You need to include that in your tolerance calculations.  

    -Francis Houde