Other Parts Discussed in Thread: TPS55288
I have a question about PSPICE simulation.
When I put an ideal capacitor on the TPS55288, I get a clean output waveform as shown below.
Figure 1(yellow dotted line)
However, when I simulate the TPS55288 with the spice model of the actual capacitor, when the output capacitor is above a certain value (176uF), the simulation data shows a switching (1.2MHz) spike voltage caused by the parasitic parameter of the capacitor, and the overshoot and undershoot are not visible under load trend.
(It doesn't look that big in the actual test).
However, if you zoom in on the spikes as shown in the figure below, you can see the overshoot and undershoot.
Figure 2(reddotted line)
Questions
1) Is this switching spike voltage a model issue with the TPS55288, as it is not when I add a real capacitor?
2) Do other DCDC simulations show the same phenomenon if I apply a lot of spice models of the capacitor?
3) Is the switching spike voltage negligible, and if so, why?