This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMQ66430-Q1: customer connect the NC to GND

Part Number: LMQ66430-Q1

Hi,

Is there any impact like EMC if customer connect NC to GND? Thank you

B&R

Yuan

  • Hi, Yuan,

    The NC pin is a No Connection Pin, and it is defined as such since it is not connected to anything internally, floating is also good.

    Pin 2,4,5,9,12 all can be left floating, and pin 5 must be floating. Because Vin is a high-voltage pin, the NC pin between the low-voltage pin and the low-voltage pin is best left floating (pin2, 4). 

    Elena