Part Number: LP5860EVM
Other Parts Discussed in Thread: LP5860, USB2ANY
Hello all,
I'm trying to set-up the LP5860 evaluation board on a windows 10 machine.
I'm using the USB2ANY adapter I got with the device as a set.
I followed all instructions of hardware/software setup.
I connected the EV board to USB2ANY device using a 30-pin ribbon cable. All jumpers are set to default.
When connecting the USB2ANY to the PC, I can see a device named "MSP430-based HID Device" under "Bluetooth & other devices".
When first entering "LP586X" software, at the bottom left of the window, there is a massage "Hardware not connected". If I press the "brackets" symbol, I get a "Connecting to TI Cloud Agent..." and it stays like this for long time, then I get a massage "GC Runtime Installation Error".
I tried installing it a couple of times, nothing helps.
Please help out, Thanks.
Attached screenshot of the error.