Hello,
I would like to ask you about the TPS61027.
Specifications are below.
I am assuming that a motor will be connected to VOUT, but are there any concerns?
Is it okay if the back electromotive force is applied to VOUT?
(Specification)
VIN: 3.0V to 5.4V
VOUT: 5V
IOUT: 100mA
Best regards,