This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5050-1-Q1: LM5050-1-Q1: Schematic review

Part Number: LM5050-1-Q1
Other Parts Discussed in Thread: LM5050-1, LM74700-Q1

hi Team,

Could you help review the schematic of Input.pdf input.pdf

The is automotive application for using Or-ing, Reverse current blocking, Reverse polarity protection.

Vin 1 & 2 = 12V

Load Current = 5A 

Revers polarity protection test voltage= -14V