This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM43600: Is the 2A variant a direct replacement for the 0.5A variant ?

Part Number: LM43600


The LM43600PWPR or LM43600QPWPR-Q1 is used in some of our products to convert 28V to 5V or 3.3V.

At the moment, our purchasing department cannot source the 0.5A variant but are able to source the 2A variant: LM43602PWPT.

I have compared the characteristics of the 0.5A variant to those of the 2A variant and I think the 2A variant can be a direct replacement for the 0.5A variant.

Am I right in thinking that? Are they any risk in doing that?

Thanks in advance for your support.

  • Hi, Gilles,

    Thank you for the posting, Yes your understand is right for this pin 2 pin device to be alternative. Please verify if inductor need to change, you can refer to DS Table 2. L, COUT and CFF Typical Values, for the components check , or if need you can also share you SCH for us to review .

    Elena

  • Hello Elena,

    Thanks for your reply.

    Could you clarify why using the 2A variant of the switcher instead of the 0.5A would require a change of the inductor?

    Is there a risk in using a 2A switcher with 0.5A inductor (the load remains unchanged compared to the 0.5A switcher)? 

    Gilles

  • Hi, Gilles,

    To ensure the optimum transient response and loop stability of the converter, a inductor is calculate with max loading and max vin condition, . If they change it to another value, they should check the performance of the device for all their operating conditions. 

    Elena

  • Thanks for your answer. Our products using the LM43600 are not a new design, there is no reason for us at this stage to change inductor values which have been used for years without problems.

    I would like to evaluate what is the risk in using the 2A variant instead of the 0.5A variant as our purchase department can source the 2A but not the 0.5A. Inductors are rated to the maximum load (<200mA) but their saturation current remains lower than the maximum current of the high side switch especially for the 2A variant:

  • Yes, truly understand your concern, suggest once you change device, check the load transient response to confirm the loop is stable, and verify theVout ripple and SW waveform stable if you do not want to change external components.

    Elena