Other Parts Discussed in Thread: TPS65981
Hi,
There are a number of GPIO events available in the TPS65981_2_7_8 Application Customization Tool (GUI version 6.1.4) which are not documented in "TPS65987D GPIO Events SLVAE11A". I am using the TPS65987DDH with a configuration template TPS65987DDH (Advanced), version 6.1.4. Events such as the following are not described in the GPIO events document:
Port 0/1 FaultZ Output Event
Port 0/1 Power Source on PC Event
Port 0/1 Power Source Ilimit Input Event
Port 0/1 FRS VBUS Discharge Event
Is there a newer version of the TPS65987D GPIO Events document that includes details of these events?
Regards,
Gerry