Hi, TI expert
Why do you recommend a pullup resistor between the values of 10kΩ and 100kΩ ?
When connected to VG+, I think that the voltage value obtained by dividing 5V with the internal resistance of the PGOOD pin and the pull-up resistance can be measured.
With that balance in mind, do you recommend 10k to 100kΩ?
If so, please tell me what the internal resistance value is in ohms.
Also, when PGOOD is high, I assume that VPGOOD = VG - RPGOOD*IPGOOD [V] is input to the IC, what is it used for?
Best regards.