Other Parts Discussed in Thread: BQSTUDIO, , EV2400
Hello! I have a BQ27421EVM-G1B board and bqStudio is reporting it as having firmware "0421_1_08_10". The firmware version bytes are "08 01".
The BQ27421 gauges that are getting stuffed onto my form-factor device PBCA are reporting firmware version bytes of "09 01".
This mismatch (EVM "08 01" vs device "09 01") is making it impossible for me to generate a Golden Image that matches my device.
How can I upgrade my BQ27421EVM-G1B to the identical firmware of my device?
As an aside: when I launch bqStudio v1.3.101 without my EV2400 plugged in, it invites me to choose the .bqz file that corresponds to my gauge. If I pick any of the "0421_1_0X_XX-bq27421GIB.bqz" files, I get a _very_ scary modal dialog box telling me that it's not supported, and that I should proceed at my own risk. Is that ok? It's scary.
Thanks,
Charles