Hi.
I am supplying the TPS5430 form a power supply in my board, which is 24VDC, 30mA.
Now, I am converting it to 3.3VDC (successfully achieved) using the reference design in datasheet.
My output load current required is 600mA.
I have to use external power supply as the on-board one is only 30mA.
Any idea, how can i increase the current in the output side , while using my on-board supply..?
Can i use a transistor from input to output as used in many voltage regulators(like one attached here)..?
Please help, thanks in advance..